Feedback_Ki

Feedback_Ki

Address: 10244 (2804H)
Type: Unsigned32
Access: Read/Write
Unit: --
Range: Unsigned32
Default Value: 1000
Store Supported: Yes
Description:

This value is used for Feedback feature and define the integral Gain of PID regulator.

The value has to be adjusted to reduce the position error (Feedback_Actual_Position_Error) or velocity error (Feedback_Actual_Velocity_Error) at the end of acceleration or deceleration.

Pay attention that a not coherent value (big value) can introduce motor vibration.

Notes: See Closed Loop Modality for details.